JAJSV55 August 2024 BQ2969
PRODUCTION DATA
The BQ2969 family of second-level protectors is used for overvoltage protection of the battery pack in the application. A regulated output is available to drive local external circuitry. The device OUT pin can be configured in one of 3 drive types and is asserted whenever the device enters the overvoltage mode. The pin is typically used to drive an NMOS FET that blows a fuse in the event of a fault condition, thereby disconnecting the pack power path.