Cell Terminate Voltage: This is the theoretical voltage where the system will begin to fail. It is defined as zero state-of-charge. Generally a more conservative level is used in order to have some reserve capacity. Note the value is for a single cell only.
Quit Current: Generally should be set to a value slightly above the expected idle current of the system.
Qmax Cell 0: Start with the C-rate value of your battery.