JAJSLN6C May 2012 – May 2021 BQ34Z100
PRODUCTION DATA
This read-word function returns an unsigned integer value of the temperature, in units of 0.1 K, measured by the gas gauge and has a range of 0 to 6553.5 K. The source of the measured temperature is configured by the [TEMPS] bit in the Pack Configuration register (see Section 7.2.2).
TEMPS | TEMPERATURE() SOURCE |
---|---|
0 | Internal Temperature Sensor |
1 | TS Input (default) |