JAJSCB3E June 2016 – April 2019 BQ35100
PRODUCTION DATA.
AltManufacturerAccess() provides a method of reading and writing data in the Manufacturer Access System (MAC). The MAC command is sent via AltManufacturerAccess() by a block protocol. The result is returned on AltManufacturerAccess() via a block read.
Commands are set by writing to registers 0x00/0x01. On a valid word access, the MAC command state is set, and commands 0x3E and 0x3F are used for MAC commands. These new addresses work the same as 0x00 and 0x01, but are primarily intended for block writes and reads.