JAJSH19I October 2013 – March 2022 BQ76920 , BQ76930 , BQ76940
PRODMIX
The performance of the cell voltage values measured by the 14-bit ADC has a factory-calibrated accuracy, as follows:
While this is suitable for the majority of pack protection and basic monitoring applications the BQ769x0 AFE family is intended to support, certain systems may require a higher accuracy performance.
To achieve this, use an available ADC channel and general purpose output terminal on the host microcontroller paired with the BQ769x0. A simple external circuit consisting of two precision resistors and a small-signal FET is activated by the host microcontroller to determine the total stack voltage, VSTACK. This is then compared against the sum of the individual cell voltages as measured by the internal ADC of the BQ769x0. The resulting transfer function coefficient, GAIN2, is simply applied to each cell voltage ADC value for improved accuracy.
The process is as follows:
As a general recommendation, a new GAIN2 function should be generated when the cell voltages increase or decrease by more than 100 mV. With GAIN2, each cell voltage calculation becomes:
For systems that do not require this additional in-use calibration function, GAIN2 is simply “1”.