JAJSSH0 December 2023 BQ77307
PRODUCTION DATA
Some device pins may not be needed in a particular application. Terminating Unused Pins shows the manner in which each pin is terminated in this case.
PIN | NAME | RECOMMENDATION |
---|---|---|
1–5, 18–20 | VC0–VC7 | Cell inputs 1 and 7 must always be connected to actual cells, with cells connected between VC1 and VC0, and between VC7 and VC6. VC0 must be connected through a resistor and capacitor on the PCB to pin 11 (VSS). Pins related to unused cells (which may be cell 2 to cell 6, pins 1–3, 20) must be shorted directly to an adjacent VC pin. All VC pins must be connected to either an adjacent VC pin or an actual cell (through R and C). |
6, 7 | SRP, SRN | If not used, connect these pins to pin 11 (VSS). |
8 | TS | If not used, connect this pin to pin 11 (VSS). |
9, 10 | DSG, CHG | If not used, leave these pins floating. |
12, 13 | SCL, SDA | If not used, connect these pins to pin 11 (VSS). |
14, 15 | ALERT, REGOUT | If not used, leave these pins floating. |
16 | REGSRC | If neither the REGOUT regulator nor the CHG and DSG drivers are used, connect this pin to pin 17 (BAT). |