JAJSSH0 December 2023 BQ77307
PRODUCTION DATA
The BQ77307 uses a special CONFIG_UPDATE mode to make changes to the data memory settings, if the device has not been SEALED by default by TI programming. If changes were made to the data memory settings while the normal protection functions were in operation, it could result in unexpected operation or consequences if settings used by the logic changed in the midst of operation. Changes to the data memory settings should generally only be done on the customer manufacturing line or in an offline condition, such as immediately after being powered from SHUTDOWN.
When in CONFIG_UPDATE mode, the device stops all protection monitoring. The host can then make changes to data memory settings. After changes are complete, the host then sends the command to exit CONFIG_UPDATE mode, at which point the device restarts normal operation using the new data memory settings. For more information, see the BQ77307 Technical Reference Manual.