JAJSSH0 December 2023 BQ77307
PRODUCTION DATA
The BQ77307 device monitors pack current using a low-side sense resistor that connects to the SRP and SRN pins through an external RC filter, which should be connected such that a charging current will create a positive voltage on SRP relative to SRN. The differential voltage between SRP and SRN is compared to programmable current protection thresholds to generate protection alerts and faults when a threshold is exceeded. The device supports independent thresholds and delay between an alert occurring and a fault being asserted for short circuit in discharge (SCD), overcurrent in discharge 1 and 2 (OCD1, OCD2), and overcurrent in charge (OCC).