JAJSSH0 December 2023 BQ77307
PRODUCTION DATA
The BQ77307 device includes two voltage references, VREF1 and VREF2, with VREF1 used by the voltage protection subsystem, which includes protections for cell overvoltage and undervoltage, temperature protections, and the VREF and VSS diagnostics. VREF2 is used by the current protection subsystem, the integrated LDOs, and the internal oscillator. The device includes a diagnostic check of VREF1 vs VREF2, such that if the ratio of the two voltages changes beyond an allowed range, a diagnostic alert or fault is triggered (if enabled by settings).