The following is the detailed design procedure.
- Based on the application current, select the proper sense resistor value. The sense resistor should allow detection of the highest current protection, short circuit current.
- Temperature protection is set with the assumption of using a 103AT NTC (or NTC with similar specification). If a different type of NTC is used, a different RTS_PU may be used for the application. Refer to the actual temperature detection threshold voltage to determine the RTS_PU value.
- Connect the CCFG pin correctly based on the number of cells in series.
- Review the Recommended Application Implementation to determine if optional components should be added to the schematic.