JAJSEZ9L march 2018 – august 2023 BQ77915
PRODUCTION DATA
A UTC fault occurs when the temperature decreases such that the voltage across an NTC thermistor gets above the UTC voltage threshold, VUTC, for a time of a UTC delay, tUTC_DELAY. CHG is turned off. The state comparator is turned on when CHG is turned off. If a discharge current is detected, the device will immediately switch the CHG back on. The response time of the state comparator is typically in 700 µs and not pose a disturbance in the discharge event. The UTC fault recovers when the voltage across thermistor gets below UTC recovery threshold, VUTC_REC, for a time of UTC delay.