SLUSE05 December 2019 BQ78350-R1A
PRODUCTION DATA.
The MRST pin controls the gas gauge reset state. The connections to this pin must be as short as possible to avoid any incoming noise. Direct connection to VCC is possible if the reset functionality is not desired or necessary.
If unwanted resets are found, one or more of the following solutions may be effective:
If a test point is added at MRST, it must be provided with a 10-kΩ series resistor.