JAJSP77A November 2019 – August 2020 BQ79600-Q1
PRODUCTION DATA
Digital reset is when digital core of the device in reset mode. It is not a power mode. Once device comes out of digital reset, [DRST] bit is set to '1', registers that are not included in NVM are set to RESET VALUE, registers included in NVM would be NVM program value. There are several conditions in which the device will go through a digital reset: