SWAS032F July 2013 – February 2015 CC3200
PRODUCTION DATA.
The CC3200 evaluation board includes a set of tools and documentation to help the user during the development phase.
The CC3200 device uses pin multiplexing extensively to accommodate the large number of peripheral functions in the smallest possible package. The PinMux tool is a utility used to select the appropriate pin multiplexing configuration that meets the end application requirements. The PinMux tool makes it easy to understand the various pin multiplexing options and enables the best configuration to be chosen without error.
The SimpleLink radio tool is a utility for operating and testing the CC3200 chipset designs during development of the application board. The CC3200 device has an auto-calibrated radio that enables easy connection to the antenna without requiring expertise in radio circuit design.
The Uniflash flash programmer utility allows end users to communicate with the SimpleLink device to update the serial flash. The easy GUI interface enables flashing of files (including read-back verification option), storage format (secured and nonsecured formatting), version reading for boot loader and chip ID, and so on.
To designate the stages in the product development cycle, TI assigns prefixes to the part numbers of the CC3200 device and support tools (see Figure 7-1).
The following documents provide support for the CC3200 device.
SWRU372 | CC3200 SimpleLink Wi-Fi and IoT Solution With MCU LaunchPad Getting Started Guide |
SWRU367 | CC3200 SimpleLink Wi-Fi and IoT Solution With MCU Technical Reference Manual |
SWRU369 | CC3200 SimpleLink Wi-Fi and IoT Solution With MCU Programmer's Guide |
SWRU370 | CC3100 and CC3200 SimpleLink Wi-Fi and IoT Solution Layout Guidelines |
SWRC289 | CC3200 SimpleLink Wi-Fi and IoT Solution With MCU LaunchPad Board Design Files |
The following links connect to TI community resources. Linked contents are provided "AS IS" by the respective contributors. They do not constitute TI specifications and do not necessarily reflect TI's views; see TI's Terms of Use.
Internet-On-a-Chip, SmartConfig, E2E are trademarks of Texas Instruments.
Cortex is a registered trademark of ARM Limited.
ARM is a registered trademark of ARM Physical IP, Inc.
Macrocell is a trademark of Kappa Global Inc.
Wi-Fi CERTIFIED is a trademark of Wi-Fi Alliance.
Wi-Fi Direct is a registered trademark of Wi-Fi Alliance.
ZigBee is a registered trademark of ZigBee Alliance.
All other trademarks are the property of their respective owners.
This integrated circuit can be damaged by ESD. Texas Instruments recommends that all integrated circuits be handled with appropriate precautions. Failure to observe proper handling and installation procedures can cause damage.
ESD damage can range from subtle performance degradation to complete device failure. Precision integrated circuits may be more susceptible to damage because very small parametric changes could cause the device not to meet its published specifications.
SLYZ022 — TI Glossary.
This glossary lists and explains terms, acronyms, and definitions.