A. CL includes probe and test-fixture capacitance.
B. Waveform 1 is for an output with internal conditions such that the output is
low, except when disabled by the output control. Waveform 2 is for an output
with internal conditions such that the output is high, except when disabled by
the output control.
C. Phase relationships between waveforms were chosen arbitrarily. All input pulses
are supplied by generators having the following characteristics: PRR ≤ 1 MHz,
ZO = 50 Ω, tr = 6 ns, tf = 6 ns.
D. For
clock inputs, fmsx is measured with the input duty cycle at
50%.
E. The
outputs are measured one at a time, with one input transition per
measurement.