JAJSSV2G March 2011 – January 2024 DAC3482
PRODUCTION DATA
Register Name | Address | Bit | Name | Function | Default Value |
---|---|---|---|---|---|
config4 | 0x04 | 15:0 | iotest_results(15:0) | This register is used with pattern checker test enabled (iotest_ena in config1, bit<15> set to 1b). It does not have a default RESET value. The values of these bits tell which bit in the word failed during the pattern checker test. iotest_results(15:8) correspond to the data bits on D[15:8] and iotest_results(7:0) correspond to the data bits on D[7:0]. | No RESET Value |