JAJSRM3 November 2023 DAC530A2W , DAC532A3W
PRODUCTION DATA
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
A1 | PVDD | Power | Power supply for the current source. Connect this pin to VDD with low trace impedance |
A2 | VOUT1 | Output | Voltage output on DAC channel 1. |
A3 | VOUT0 | Output | Voltage output on DAC channel 0. |
A4 | GPIO/SDO | Input/Output | General-purpose input/output configurable as LDAC, PD, PROTECT, RESET, SDO, and STATUS. For STATUS and SDO, connect the pin to the I/O voltage with an external pullup resistor. If unused, connect the GPIO/SDO pin to VDD or AGND using an external resistor. This pin can ramp up before VDD. |
B1 | VDD | Power | Supply voltage. |
B2 | FB1 | Input | Voltage feedback pin for channel 1. In voltage-output mode, connect to VOUT1 for closed-loop amplifier output. Use this pin as analog input in comparator mode. |
B3 | PGND | Ground | Ground return path for the current source. Connect this pin to AGND. |
B4 | SCL/SYNC | Output | I2C serial interface clock or SPI chip select input. This pin must be connected to the I/O voltage using an external pullup resistor. This pin can ramp up before VDD. |
C1 | AGND | Ground | Ground reference point for all circuitry on the device. |
C2 | PVDD | Power | Power supply for the current source. Connect this pin to VDD. |
C3 | IOUT | Output | Current output on channel 2. |
C4 | A0/SDI | Input | Address
configuration pin for I2C or serial data input for SPI.
For A0, connect this pin to VDD, AGND, SDA, or SCL for address configuration (see the Address Byte section). For SDI, this pin need not be pulled up or pulled down. This pin can ramp up before VDD. |
D1 | CAP | Power | External bypass capacitor for the internal LDO. Connect a capacitor (approximately 1.5 μF) between CAP and AGND. |
D2 | PVDD | Power | Power supply for the current source. Connect this pin to VDD. |
D3 | IOUT | Output | Current output on channel 2. |
D4 | SDA/SCLK | Input/Output | Bidirectional I2C serial data bus or SPI clock input. This pin must be connected to the I/O voltage using an external pullup resistor in the I2C mode. This pin can ramp up before VDD. |
PIN | TYPE | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
A1 | PVDD | Power | Power supply for the current source. Connect this pin to VDD with low trace impedance |
A2 | VOUT1 | Output | Voltage output on DAC channel 1. |
A3 | NC | -- | Solder this ball to the pad. |
A4 | GPIO/SDO | Input/Output | General-purpose input/output configurable as LDAC, PD, PROTECT, RESET, SDO, and STATUS. For STATUS and SDO, connect the pin to the I/O voltage with an external pullup resistor. If unused, connect the GPIO/SDO pin to VDD or AGND using an external resistor. This pin can ramp up before VDD. |
B1 | VDD | Power | Supply voltage. |
B2 | FB1 | Input | Voltage feedback pin for channel 1. In voltage-output mode, connect to VOUT1 for closed-loop amplifier output. Use this pin as analog input in comparator mode. |
B3 | PGND | Ground | Ground return path for the current source. Connect this pin to AGND. |
B4 | SCL/SYNC | Output | I2C serial interface clock or SPI chip select input. This pin must be connected to the I/O voltage using an external pullup resistor. This pin can ramp up before VDD. |
C1 | AGND | Ground | Ground reference point for all circuitry on the device. |
C2 | PVDD | Power | Power supply for the current source. Connect this pin to VDD. |
C3 | IOUT | Output | Current output on channel 2. |
C4 | A0/SDI | Input | Address
configuration pin for I2C or serial data input for SPI.
For A0, connect this pin to VDD, AGND, SDA, or SCL for address configuration (see the Address Byte section). For SDI, this pin need not be pulled up or pulled down. This pin can ramp up before VDD. |
D1 | CAP | Power | External bypass capacitor for the internal LDO. Connect a capacitor (approximately 1.5 μF) between CAP and AGND. |
D2 | PVDD | Power | Power supply for the current source. Connect this pin to VDD. |
D3 | IOUT | Output | Current output on channel 2. |
D4 | SDA/SCLK | Input/Output | Bidirectional I2C serial data bus or SPI clock input. This pin must be connected to the I/O voltage using an external pullup resistor in the I2C mode. This pin can ramp up before VDD. |