JAJSES9 February 2018 DAC8771
PRODUCTION DATA.
The DAC8771 implements an alarm action register (address 0x0D,). By writing to this register, the user can select the action that the device takes automatically in case of a specific alarm condition. If different setting are chosen for different alarm conditions, the following priority (high to low) is considered when taking action:
This device also contains a 6 bit alarm code register (address 0x0E Table 5) which can be loaded to the DAC if the alarm action register is set to "01". Note that the alarm code, once set, remains set even if the alarm condition is removed. Also note that the alarm action change to the programmed code is a step function even if slew rate control is enabled.