JAJSN51C november 2021 – july 2023 DLP160AP
PRODUCTION DATA
A pico projector is created by using a DLP chipset comprised of a DMD, a DLPC3420 controller, and a DLPA2000/2005 PMIC/LED driver. The DLPC3420 controller performs the digital image processing, the DLPA2000/2005 provides the needed analog functions for the projector, and the DMD is the display device for producing the projected image.
In addition to the three DLP chips in the chipset, other chips are needed. At a minimum a flash part is needed to store the DLPC3420 controller software.
The illumination light that is applied to the DMD is typically from red, green, and blue LEDs. These are often contained in three separate packages, but sometimes more than one color of LED die may be in the same package to reduce the overall size of the pico projector.
The DLPC3420 controller receives image data from the multimedia front end over a 24-bit parallel interface. An I2C interface should be connected from the multimedia front end for sending commands to the DLPC3420 controller for configuring the chipset for different features.