JAJSLH9A March 2021 – May 2022 DLP650TE
PRODUCTION DATA
The DMD features a built-in thermal diode that measures the temperature at one corner of the die outside the micromirror array. The thermal diode can be interfaced with the TMP411 temperature sensor as shown in Figure 8-4. The software application contains functions to configure the TMP411 to read the DLP650TE DMD temperature sensor diode. This data can be leveraged by the customer to incorporate additional functionality in the overall system design such as adjusting illumination, fan speeds, and so on. All communication between the TMP411 and the DLPC7540 controller happens over the I2C interface. The TMP411 connects to the DMD via pins outlined in Table 5-1.
Leave TEMP_N and TEMP_P pins unconnected (NC) if the temp sensor is not used.