JAJSFX3F august 2012 – april 2023 DLP9500
PRODUCTION DATA
The DLP9500 DMD is well suited for visible light applications requiring fast, spatially programmable light patterns using the micromirror array. See the block diagram in Figure 7-1 to see the connections between the DLP9500 DMD, the DLPC410 digital controller, the DLPR410 EEPROM, and the DLPA200 DMD micromirror drivers. An example application block diagram can be found in Figure 8-1. Layout guidelines should be followed for reliability.