JAJSRE8A October 2015 – September 2023 DLPA3000
PRODUCTION DATA
The chip temperature is constantly monitored to prevent overheating of the device. There are two levels of a fault condition. The first is TS_WARN (0x0C, bit 0) to warn for overheating. This is an indication that the chip temperature raises to a critical temperature. The next level of warning is TS_SHUT(0x0C, bit 1). This occurs at a higher temperature than TS_WARN (0x0C, bit 0) and shuts down the chip to prevent permanent damage. Both temperature faults have hysteresis on their levels to prevent rapid switching around the temperature threshold.