JAJSNS3A October 2015 – February 2023 DLPA3005
PRODUCTION DATA
This block contains all the supplies needed for the DMD and DLPC (Figure 7-12). The block comprises:
The DMD supplies block is designed to work with the DMD and the related DLPC. The DMD has its own set of supply voltage requirements. Besides the three high voltages, two supplies are needed for the DMD and the related DLPC (DLPC343x-family for instance). These supplies are made by two buck converters.
The EEPROM of the DLPA3005 is factory programmed for a certain configuration, such as which buck converters are used. Which configuration is programmed in EEPROM can be read in the capability register. It concerns the following bits: