JAJSNS3A October 2015 – February 2023 DLPA3005
PRODUCTION DATA
The power-up and power-down sequence is important to ensure a correct operation of the DLPA3005 and to prevent damage to the DMD. The DLPA3005 controls the correct sequencing of the DMD_VRESET, DMD_VBIAS, and DMD_VOFFSET to ensure a reliable operation of the DMD.
The general startup sequence of the supplies is described earlier in Section 7.3.1. The power-up sequence of the high voltage DMD lines is especially important in order not to damage the DMD. A too large delta voltage between DMD_VBIAS and DMD_VOFFSET could cause the damage and should therefore be prevented.
After PROJ_ON is pulled high, the DMD buck converters and LDOs are powered (PWR1-4) the DMD high voltage lines (HV) are sequentially enabled. First, DMD_VOFFSET is enabled. After a delay VOFS_STATE_DURATION, DMD_VBIAS is enabled. Finally, again after a delay VBIAS_STATE_DURATION, DMD_VRESET is enabled. Now the DLPA3005 is fully powered and ready for starting projection.
For power down there are two sequences, normal power down (Figure 9-1) and a fault fast power down used in case a fault occurs (Figure 9-2).
In normal power down mode, the power down is initiated after pulling PROJ_ON pin low. 25 ms after PROJ_ON is pulled low, first DMD_VBIAS and DMD_VRESET stop regulating, 10 ms later followed by DMD_VOFFSET. When DMD_VOFFSET stopped regulating, RESET_Z is pulled low. 1 ms after the DMD_VOFFSET stopped regulating, all three voltages are discharged. Finally, all other supplies are turned off. INT_Z remains high during the power down sequence since no fault occurred. During power down it is ensured that the HV levels do not violate the DMD specifications on these three lines. For this it is important to select the capacitors such that CVOFFSET is equal to CVRESET and CVBIAS is ≤ CVOFFSET, CVRESET.
The fast power down mode (Figure 9-2) is started in case a fault occurs (INT_Z will be pulled low), for instance due to overheating. The fast power down mode can be enabled / disabled through register 0x01, FAST_SHUTDOWN_EN. By default the mode is enabled. After the fault occurs, regulation of DMD_VBIAS and DMD_VRESET is stopped. The time (delay) between fault and stop of regulation can be controlled through register VBIAS/VRST_DELAY. The delay can be selected between 4 µs and ≅1.1 ms, where the default is ≅540 µs. A defined delay-time after the regulation stopped, all three high voltages lines are discharged and RESET_Z is pulled low. The delay can be controlled through register VOFS/VRESETZ_DELAY. Delay can be selected between 4 µs and ≅1.1ms. The default is ≅4 µs. Finally the internal DMD_EN signal is pulled low.
The DLPA3005 is now in a standby state. It remains in standby state until the fault resolves. In case the fault resolves, a restart is initiated. It starts then by powering-up PWR_3 and follows the regular power up, as depicted in Figure 9-2. For proper discharge timing and levels, select the capacitors such that CVOFFSET is equal to CVRESET and CVBIAS is ≤ CVOFFSET, CVBIAS.