4 Revision History
Changes from Revision D (June 2019) to Revision E (November 2020)
- 文書全体の表、図、相互参照の採番方法を更新Go
- 一般的なデータシートのフォーマットと注文情報を更新Go
- ピクセル・クロック仕様の上限を 155MHz に変更。Go
- サポートされている PMIC に DLPA3005 を追加し、PMIC 製品フォルダへのリンクを追加Go
- Changed layout of pinout maps to improve readability for
user.Go
- Deleted mention of mirror parking time from PARKZ pin description and moved to a specification tableGo
- Changed JTAG pin names from reserved to proper names Go
- Deleted support for adjustable DATAEN_CMD polarity Go
- Deleted mention of a specific 3D command Go
- Deleted support for adjusting PCLK capture edge in software Go
- Changed the description of how to use the CMP_OUT pin and corrected how the
comparator must use GPIO_10 (RC_CHARGE) instead of CMP_PWM Go
- Deleted support for CMP_PWMGo
- Added note about VCC_INTF power up recommendations if secondary devices are
on the I2C bus Go
- Deleted mention of unsupported keypad inputs Go
- Corrected optional MTR_SENSE support to GPIO_18 instead of GPIO_19 Go
- Deleted mention of unsupported light sensor on GPIO_13 and GPIO_12 Go
- Deleted reference of the RC_CHARGE circuit being used for the light sensor
and added reference of it being used for the thermistor Go
- Deleted reference of the LS_PWR circuit being used for the light
sensorGo
- Deleted mention of the unsupported LABB output sample and hold sensor
control signalGo
- Clarified GPIO_03 - GPIO_01 pins are required to be used as a SPI1
portGo
- Deleted misleading note about GPIO pins defaulting to inputs Go
- Corrected how pins are mentioned that are only available on the
DLPC3438Go
- Added missing I/O definition 10 Go
- Deleted unneeded VCC_INTF and VCC_FLSH absolute maximum values Go
- Added high voltage tolerant note to Absolute Maximum Ratings table Go
- Changed incorrect pin tolerance Go
- Changed Power Electrical Characteristics table to reflect updated power measurement values and techniques Go
- Added note that the power numbers vary depending on the utilized softwareGo
- Changed and fixed incorrect test conditions for current drive strengthsGo
- Deleted redundant ǀVODǀ specification which is referenced in later sectionsGo
- Added minimum and maximum values for VOH for I/O type 4Go
- Added minimum and maximum values for VOL for I/O type 4Go
- Deleted incorrect reference to 2.5-V, 24-mA drive Go
- Corrected I2C buffer test conditionsGo
- Deleted incorrect steady-state common mode voltage reference Go
- Changed high voltage tolerant I/O note to only refer to the I2C buffer and changed VCC to VCC_INTF.Go
- Added |VOD| minimum and maximum values, and changed the typical valueGo
- Added high-level output voltage minimum and maximum values for the sub-LVDS DMD interface, deleted redundant mention of specification, and changed the typical value Go
- Added low-level output voltage minimum and maximum values for the sub-LVDS DMD interface, deleted redundant mention of specification, and changed the typical value Go
- Corrected the name of the DMD Low-Speed signals from inputs to outputs Go
- Deleted VOH(DC) maximum and VOL(DC) minimum valuesGo
- Added note about DMD input specs being met if a proper series termination resistor is used Go
- Deleted reference of selecting unsupported oscillator frequency Go
- Corrected system oscillator clock period to match clock frequency Go
- Changed pulse duration percent spec from a maximum to a minimum Go
- Added condition for VDD rise time Go
- Deleted the incorrect part of the tp_tvb definitionGo
- Deleted unneeded total horizontal blanking equation Go
- Changed minimum total vertical blanking equation Go
- Increased maximum PCLK from 150 MHz to 155 MHz Go
- Deleted reference to various signal's active edges being configurable Go
- Changed the minimum flash SPI_CLK frequencyGo
- Corrected flash interface clock period to match clock frequency Go
- Added Section 6.17 section to more clearly list signal transition time requirementsGo
- Changed GPIO_08 (PROJ_ON) pulse width requirement and added a requirement to keep GPIO_08 high until HOST_IRQ goes low Go
- Changed DMD HS clock switching rate from maximum to nominal and added accompanying clock specification Go
- Added Section 6.19 sectionGo
- Added the Section 6.20 section to clarify chipset support requirementsGo
- Changed how chipset support is mentioned in the Detailed Description section Go
- Deleted support for 3D video over DSI Go
- Deleted reference to internal software tools and clarified how firmware affects the supported resolution and frame rates Go
- Added note stating bits per pixel limitation at 120 Hz with DSI inputGo
- Added note that up to four DSI lanes may be required to fully utilize the bandwidth Go
- Deleted mention of sequencer sync mode as its generally assumed to be autoGo
- Clarified note about VSYNC_WE needing to remain active Go
- Deleted support for changing the clock active edge and clarified support of changing the sync active edgeGo
- Changed the DATAEN_CMD signal to not be optional Go
- Added note that LP mode is required during vertical time for DSI Go
- Changed requirement related to DSI initialization Go
- Deleted incorrect DSI data type; see software programmers guide
instead.Go
- Added information that the parallel interface isn't ready to accept data until the auto-initialization process is completedGo
- Changed how the 500 ms startup time is described Go
- Changed SPI flash key timing parameter access frequency minimum and maximum valuesGo
- Changed maximum flash size supported from 16 Mb to 128 Mb Go
- Deleted SPI signal routing section Go
- Deleted support for a light sensor integrated with the DLPC34xx
controller Go
- Added missing timing definitions Go
- Clarified that the mentioned SDR clock speed is the typical
valueGo
- Changed the description of how PROJ_ON affects the power supplies Go
- Changed which signals are listed as tri-stated at power up and which signals are pulled low Go
- Changed 1-oz copper plane recommendation Go
- Deleted reference to unsupported option of variable frequency
reference clockGo
- Added additional DMD data and DMD clock signal matching requirements Go
- Changed maximum mismatch from ±0.1" to ±1.0" Go
- Changed incorrect signal matching requirement table noteGo
- Changed differential signal layer change to a recommendationGo
- Changed wording requiring no more than two vias on certain DMD
signals Go
- Changed the package designator description for the DLPC3433 to match the actual packageGo
- Changed device markings image and definitions Go
Changes from Revision C (December 2016) to Revision D (June 2019)
- Changed mirror parking time from "500 μs" to "20 ms" for PARKZ description in Pin Functions tableGo
Changes from Revision A (September 2014) to Revision B (January 2016)
- Moved the storage temperature to theAbsolute Maximum Ratings table Go
- Updated the Handling Ratings table to an ESD Ratings table Go
- Updated Section 11.1.2.1 image and tableGo
Changes from Revision * (February 2014) to Revision A (September 2014)
- デバイスの状態を「製品プレビュー」から「量産データ」へ変更し、ドキュメントの完全版をリリースGo