JAJSN65A October 2019 – October 2021 DRV10982-Q1
PRODUCTION DATA
A fast change in the applied drive current may result in a sudden change in the driving torque. In some applications, this could result in acoustic noise. To avoid this, the DRV10982-Q1 device allows the option of limiting the rate at which the current is applied to the motor. OpLCurrRt[2:0] sets the maximum voltage ramp-up rate that is applied to the motor. The waveforms in #SLVSCP22480 show how this feature can be used to gradually ramp the current applied to the motor.
![]() | ![]() |
Start driving with fast current ramp | Start driving with slow current ramp |