JAJSEM5 February 2019 DRV5021-Q1
PRODUCTION DATA.
If the device is powered on with a magnetic field strength between BRP and BOP, then the device output is indeterminate. If the field strength is greater than BOP, then the output is pulled low. If the field strength is less than BRP, then the output is released.