JAJSHT7 August 2019 DRV5057-Q1
PRODUCTION DATA.
If an analog signal is needed at the end of a large travel distance, first use a microcontroller to digitally decode the PWM, then use a DAC to produce the analog signal. If an analog signal is needed after a short signal travel distance, use an analog output device, such as the DRV5055-Q1.
If an analog signal is needed at the end of a large travel distance and a microcontroller is unavailable, use a low-pass filter to convert the PWM signal into an analog voltage, as shown in Figure 17. When using this method, note the following: