JAJSSE7 November 2023 DRV8214
PRODUCTION DATA
In the fixed off-time mode, the H-bridge enters a brake/low-side slow decay state (both low-side MOSFETs ON) for tOFF duration after IOUT exceeds ITRIP. After tOFF the outputs are re-enabled according to the control inputs unless IOUT is still greater than ITRIP. If IOUT is still greater than ITRIP, the H-bridge will enter another period of brake/low-side slow decay for tOFF. If the state of the EN/IN1 or PH/IN2 control pin inputs or I2C_EN_IN1 or I2C_PH_IN2 bits changes during the tOFF time, the remainder of the tOFF time is ignored, and the outputs will again follow the inputs.
The fixed off-time mode allows for a simple current regulation scheme independent of the external controller. Fixed off-time mode will support 100% duty cycle current regulation since the H-bridge automatically enables after the tOFF period and does not require a new control input edge on the control input pins or bits to reset the outputs.