JAJSSE7 November 2023 DRV8214
PRODUCTION DATA
The DRV8214 allows the nFAULT pin to be configured for various settings of RC_CNT using the RC_REP register. Table 8-21 lists the settings for the RC_REP register (refer to Section 8.6 for details). Timing diagrams corresponding to RC_REP settings are shown in Figure 8-13 and Figure 8-14.
RC_REP |
nFAULT |
RC_CNT |
---|---|---|
00b |
Ripple counting has no effect on nFAULT |
If RC_CNT reaches the maximum value of 216 - 1, it is held at that value until a CLR_CNT command is issued. |
01b |
Ripple counting has no effect on nFAULT |
If RC_CNT reaches the maximum value of 216 - 1, RC_CNT is cleared and restarted from 0. |
10b |
nFAULT is pulled low if RC_CNT exceeds threshold |
If RC_CNT reaches the maximum value of 216 - 1, it is held at that value until a CLR_CNT command is issued. |
11b |
nFAULT is pulled low for 50 μs if RC_CNT reaches the maximum value of 216 - 1 |
If RC_CNT reaches the maximum value of 216 - 1, RC_CNT is cleared and restarted from 0. |