JAJSSE7 November 2023 DRV8214
PRODUCTION DATA
EC_MISS_PER is a 2-bit register that allows the user to select a time window for when a current ripple is expected to be detected. During this time window, the error corrector takes action if an expected ripple from the digital filter does not arrive. The time window is represented as a percentage of time between two successive expected current ripples. The settings are shown in :
Bit | Value |
---|---|
00b | 20% |
01b | 30% |
10b | 40% |
11b | 50% |