JAJSU38 April 2024 DRV8215
PRODUCTION DATA
Denoted by INV_R_SCALE, this is the scaling factor for the inverse of motor resistance (INV_R). Since the inverse of a motor resistance is generally not an integer, the value must be rounded off to the nearest integer. Settings are described in Table 7-17.
Bit | Value of INV_R_SCALE |
---|---|
00b | 2 |
01b | 64 |
10b | 1024 |
11b | 8192 |
INV_R is represented by the equation:
Please note that the maximum value of INV_R is 255. Please refer to Section 9.2.3.1.1 for an example on how to select the appropriate INV_R_SCALE for a given value of motor resistance.