JAJSSJ5 December 2023 DRV8234
PRODUCTION DATA
EC_MISS_PERis a 2-bit register that allows the user to select a time window for when a current ripple is expected to be detected. During this time window, the error corrector identifies any ripples filtered out from the digital filter to classify them as missed and adds them manually. The time window is represented as a percentage of time between two successive expected current ripples. During this time window, the error corrector takes action if an expected ripple from the digital filter does not arrive. The time window is represented as a percentage of time between two successive expected current ripples. The settings are shown in Table 8-7:
Bit | Value |
---|---|
00b | 20% |
01b | 30% |
10b | 40% |
11b | 50% |