JAJSSJ5 December 2023 DRV8234
PRODUCTION DATA
Denoted by RC_THR_SCALE, this is the scaling factor for the number of ripples for threshold. Settings are given below.
Bit | Value of RC_THR_SCALE |
---|---|
00b | 2 |
01b | 8 |
10b | 16 |
11b | 64 |
Depending on the number of ripples per revolution, NR, and the speed of rotations, RC_THR_SCALE can be chosen high or low based on user requirement of the nFAULT pin. If total number of ripple counts until the end of an operation cycle are low, choose a lower value of RC_THR_SCALE, otherwise a higher value is recommended.
Please note that RC_THR and RC_THR_SCALE do not affect the accuracy of ripple counting.