JAJSGI8D April 2016 – October 2019 DS90UB914A-Q1
PRODUCTION DATA.
I2C pass-through provides a way to access remote devices at the other end of the FPD-Link III interface. This option is used to determine if an I2C instruction is transferred over to the remote I2C bus. For example, when the I2C master is connected to the deserializer and I2C pass-through is enabled on the deserializer, any I2C traffic targeted for the remote serializer or remote slave will be allowed to pass through the deserializer to reach those respective devices.
See Figure 25 for an example of this function and refer to application note: I2C over DS90UB913/4 FPD-Link III with Bidirectional Control Channel (SNLA222).
If master controller transmits I2C transaction for address 0xA0, the DES A with I2C pass-through enabled will transfer I2C commands to remote Camera A. The DES B with I2C pass-through disabled, any I2C commands will NOT be passed on the I2C bus to Camera B.