7 |
GPIO6_OUTPUT
_VALUE |
R/W |
0h |
Local GPIO Output Value.
This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is Output, and remote GPIO control is disabled. |
6 |
GPIO6_REMOTE
_ENABLE |
R/W |
0h |
Remote GPIO Control.
1: Enable GPIO control from remote Serializer. The GPIO pin will be an output, and the value is received from the remote Serializer.
0: Disable GPIO control from remote Serializer. |
5 |
GPIO6_DIR |
R/W |
0h |
The GPIO DIR configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
4 |
GPIO6_EN |
R/W |
0h |
The GPIO EN configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
3 |
GPIO5_OUTPUT
_VALUE |
R/W |
0h |
Local GPIO Output Value.
This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is Output, and remote GPIO control is disabled. |
2 |
GPIO5_REMOTE
_ENABLE |
R/W |
0h |
Remote GPIO Control.
1: Enable GPIO control from remote Serializer. The GPIO pin will be an output, and the value is received from the remote Serializer.
0: Disable GPIO control from remote Serializer. |
1 |
GPIO5_DIR |
R/W |
0h |
The GPIO DIR configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
0 |
GPIO5_EN |
R/W |
0h |
The GPIO EN configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |