8.6.1.11 SlaveID_2 Register (Address = Ah) [reset = 0h]
SlaveID_2 is described in Table 22.
Return to Summary Table.
Table 22. SlaveID_2 Register Field Descriptions
Bit |
Field |
Type |
Reset |
Description |
7-1 |
SLAVE_ID2 |
R/W |
0h |
7-bit Remote Slave Device ID 2.
Configures the physical I2C address of the remote I2C Slave device attached to the remote Serializer. If an I2C transaction is addressed to the Slave Alias ID2, the transaction will be remapped to this address before passing the transaction across the Bidirectional Control Channel to the Serializer. |
0 |
RESERVED |
R/W |
0h |
Reserved |