7-4 |
Rev-ID |
R |
0h |
Revision ID
0100: DS90UH940-Q1
0110: DS90UH940N-Q1 |
3 |
GPIO0_OUTPUT
_VALUE
_D_GPIO0_OUTPUT
_VALUE |
R/W |
0h
0h |
Local GPIO Output Value
This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is Output, and remote GPIO control is disabled. |
2 |
GPIO0_REMOTE
_ENABLE
_D_GPIO0_REMOTE
_ENABLE |
R/W |
0h
0h |
Remote GPIO Control
1: Enable GPIO control from remote Serializer. The GPIO pin will be an output, and the value is received from the remote Serializer.
0: Disable GPIO control from remote Serializer. |
1 |
GPIO0_DIR
_D_GPIO0_DIR |
R/W |
0h
1h |
The GPIO DIR configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
0 |
GPIO0_EN
_D_GPIO0_EN |
R/W |
0h
1h |
The GPIO EN configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |