JAJSMG0C june 2021 – december 2022 HDC3020 , HDC3021 , HDC3022
PRODUCTION DATA
An I2C read sequence is performed to retrieve data from the HDC302x. The I2C read sequence must follow the I2C write sequence that was used to initiate the data acquisition. A CRC byte always accompanies data that is transmitted by the HDC302x. If the I2C controller does not use the CRC byte to perform a data integrity check, then an I2C NACK can be issued to discard CRC transmission and save time. Both of these I2C read scenarios are illustrated in Figure 8-5 and Figure 8-6.
The HDC302x will stop transmission of a data byte if the I2C controller fails to ACK after any byte of data.