JAJSSL1A October 1997 – December 2024 INA122
PRODUCTION DATA
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The input impedance of the INA122 is extremely high, approximately 1010Ω. However, a path must be provided for the input bias current of both inputs. This input bias current is approximately −10nA (current flows out of the input terminals). High input impedance means that the input bias current changes very little with varying input voltage.
Input circuitry must provide a path for this input bias current for proper operation. Figure 7-2 shows various provisions for an input bias current path. Without a bias current path, the inputs can float to a potential which exceeds the common-mode range of the INA122 and the input amplifiers saturate.
If the differential source resistance is low, the bias current return path can be connected to one input (see the thermocouple example in Figure 7-2). With higher source impedance, using two equal resistors provides a balanced input with possible advantages of lower input offset voltage due to bias current and better high-frequency common-mode rejection.