The INA185-Q1 is in normal operation when the following conditions are met:
- The power supply voltage (VS) is
between 2.7V and 5.5V.
- The common-mode voltage (VCM) is
within the specified range of –0.2V to 26V.
- The maximum differential input signal multiplied
by the gain plus VREF is less than VS minus the output voltage swing
to VS.
- The minimum differential input signal multiplied
by the gain plus VREF is greater than the swing to GND (see the Rail-to-Rail Output Swing section).
During normal operation, these devices produce an output voltage that is the gained-up representation of the difference voltage from IN+ to IN– plus the reference voltage at VREF.