JAJSR73 February 2024 INA185-Q1
PRODUCTION DATA
When used in low-side current sensing applications, the offset voltage of the INA185-Q1 is within ±55µV for A2, A3 and A4 devices. The low offset performance of the INA185-Q1 has two main benefits. First, the low offset allows these devices to be used in applications that must measure current over a wide dynamic range. In this case, the low offset improves the accuracy when the sensed currents are on the low end of the measurement range. The other advantage of low offset is the ability to sense lower voltage drop across the sense resistor accurately, thus allowing a lower-value shunt resistor. Lower-value shunt resistors reduce power loss in the current sense circuit, and help improve the power efficiency of the end application.
The gain error of the INA185-Q1 is specified to be within 0.2% of the actual value for A1, A2, and A3 devices. As the sensed voltage becomes much larger than the offset voltage, this voltage becomes the dominant source of error in the current sense measurement.