JAJSON6A July 2023 – December 2023 INA740A , INA740B
PRODMIX
Table 7-5 lists the INA740x registers. All register locations not listed in Table 7-5 should be considered as reserved locations and the register contents should not be modified.
Address |
Acronym | Register Name | Register Size (bits) | Section |
---|---|---|---|---|
0h | CONFIG | Configuration | 16 | Go |
1h | ADC_CONFIG | ADC Configuration | 16 | Go |
5h | VBUS | Bus Voltage Measurement | 16 | Go |
6h | DIETEMP | Temperature Measurement | 16 | Go |
7h | CURRENT | Current Result | 16 | Go |
8h | POWER | Power Result | 24 | Go |
9h | ENERGY | Energy Result | 40 | Go |
Ah | CHARGE | Charge Result | 40 | Go |
Bh | DIAG_ALRT | Diagnostic Flags and Alert | 16 | Go |
Ch | COL | Current Over-Limit Threshold | 16 | Go |
Dh | CUL | Current Under-Limit Threshold | 16 | Go |
Eh | BOVL | Bus Overvoltage Threshold | 16 | Go |
Fh | BUVL | Bus Undervoltage Threshold | 16 | Go |
10h | TEMP_LIMIT | Temperature Over-Limit Threshold | 16 | Go |
11h | PWR_LIMIT | Power Over-Limit Threshold | 16 | Go |
3Eh | MANUFACTURER_ID | Manufacturer ID | 16 | Go |
Complex bit access types are encoded to fit into small table cells. Table 7-6 shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
Reset or Default Value | ||
-n | Value after reset or the default value |
The CONFIG register is shown in Table 7-7.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | RST | R/W | 0h | Reset Bit. Setting this bit to '1' generates a system
reset that is the same as power-on reset. Resets all registers to default values. 0h = Normal Operation 1h = System Reset sets registers to default values This bit self-clears. |
14 | RSTACC | R/W | 0h | Resets the contents of accumulation registers ENERGY
and CHARGE to 0 0h = Normal Operation 1h = Clears registers to default values for ENERGY and CHARGE registers |
13-6 | CONVDLY | R/W | 0h | Sets the Delay for initial ADC conversion in steps of
2 ms. 0h = 0 s 1h = 2 ms FFh = 510 ms |
5 | RESERVED | R | 0h | Reserved. Always reads 0. |
4 | RESERVED | R | 1h | Reserved. Always reads 1. |
3-0 | RESERVED | R | 0h | Reserved. Always reads 0. |
The ADC_CONFIG register is shown in Table 7-8.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-12 | MODE | R/W | Fh | The user can set the MODE bits for continuous or
triggered mode on bus voltage, shunt voltage or temperature
measurement. 0h = Shutdown 1h = Triggered bus voltage, single shot 2h = Reserved 3h = Reserved 4h = Triggered temperature, single shot 5h = Triggered temperature and bus voltage, single shot 6h = Triggered temperature and current, single shot 7h = Triggered temperature, current and bus voltage, single shot 8h = Shutdown 9h = Continuous bus voltage only Ah = Reserved Bh = Reserved Ch = Continuous temperature only Dh = Continuous bus voltage and temperature Eh = Continuous temperature and current Fh = Continuous temperature, current, and bus voltage |
11-9 | VBUSCT | R/W | 5h | Sets the conversion time of the bus voltage
measurement. 0h = 50 µs 1h = 84 µs 2h = 150 µs 3h = 280 µs 4h = 540 µs 5h = 1052 µs 6h = 2074 µs 7h = 4120 µs |
8-6 | VSENCT | R/W | 5h | Sets the conversion time of the shunt resistor
voltage. Works in conjunction with the temperature conversion time.
Total conversion time for a current measurement is the sum of VSENCT
and TCT selections. 0h = 50 µs 1h = 84 µs 2h = 150 µs 3h = 280 µs 4h = 540 µs 5h = 1052 µs 6h = 2074 µs 7h = 4120 µs |
5-3 | TCT | R/W | 5h | Sets the conversion time of the temperature
measurement. Works in conjunction with the shunt voltage conversion
time for current measurements. Total conversion time for a current
measurement is the sum of VSENCT and TCT selections. 0h = 50 µs 1h = 84 µs 2h = 150 µs 3h = 280 µs 4h = 540 µs 5h = 1052 µs 6h = 2074 µs 7h = 4120 µs |
2-0 | AVG | R/W | 0h | Selects ADC sample averaging count. The averaging
setting applies to all active inputs. When >0h, the output registers are updated after the averaging has completed. 0h = 1 1h = 4 2h = 16 3h = 64 4h = 128 5h = 256 6h = 512 7h = 1024 |
The VBUS register is shown in Table 7-9.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | VBUS | R | 0h | Bus voltage output. Two's complement
value, however always positive. Conversion factor: 3.125 mV/LSB |
The DIETEMP register is shown in Table 7-10.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-4 | DIETEMP | R | 0h | Internal die temperature measurement.
Two's complement value. Conversion factor: 125 m°C/LSB |
3-0 | RESERVED | R | 0h | Reserved. Always reads 0. |
The CURRENT register is shown in Table 7-11.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | CURRENT | R | 0h | Calculated current output in Amperes.
Two's complement value. Conversion factor: 1.2 mA/LSB. |
The POWER register is shown in Table 7-12.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
23-0 | POWER | R | 0h | Calculated power output. Output value in Watts. Unsigned representation. Positive value. Conversion factor: 240 μW/LSB. |
The ENERGY register is shown in Table 7-13.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
39-0 | ENERGY | R | 0h | Calculated energy output. Output value is in Joules.Unsigned representation. Positive value. Conversion factor: 3.84 mJ/LSB. |
The CHARGE register is shown in Table 7-14.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
39-0 | CHARGE | R | 0h | Calculated charge output. Output value is in
Coulombs.Two's complement value. Conversion factor: 75 μC//LSB. |
The DIAG_ALRT register is shown in Table 7-15.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | ALATCH | R/W | 0h | When the Alert Latch Enable bit is set to Transparent
mode, the Alert pin and Flag bit reset to the idle state when the
fault has been cleared. When the Alert Latch Enable bit is set to Latch mode, the Alert pin and Alert Flag bit remain active following a fault until the DIAG_ALRT Register has been read. 0h = Transparent 1h = Latched |
14 | CNVR | R/W | 0h | Setting this bit high configures the Alert pin to be
asserted when the Conversion Ready Flag (bit 1) is asserted,
indicating that a conversion cycle has completed. 0h = Disables conversion ready flag on ALERT pin 1h = Enables conversion ready flag on ALERT pin |
13 | SLOWALERT | R/W | 0h | When enabled, ALERT function is asserted on the
completed averaged value. This gives the flexibility to delay the ALERT until after the averaged value. 0h = ALERT comparison on non-averaged (ADC) value 1h = ALERT comparison on averaged value |
12 | APOL | R/W | 0h | Alert Polarity bit sets the Alert pin polarity. 0h = Normal (active-low, open-drain) 1h = Inverted (active-high, open-drain ) |
11 | ENERGYOF | R | 0h | This bit indicates the health of the ENERGY register.
If the 40-bit ENERGY register has overflowed this bit is set to 1. 0h = Normal 1h = Overflow Clears by setting the RSTACC field in the Configuration register. |
10 | CHARGEOF | R | 0h | This bit indicates the health of the CHARGE
register. If the 40-bit CHARGE register has overflowed this bit is set to 1. 0h = Normal 1h = Overflow Clears by setting the RSTACC field in the Configuration register. |
9 | MATHOF | R | 0h | This bit is set to 1 if an arithmetic operation
resulted in an overflow error. It indicates that current and power data may be invalid. 0h = Normal 1h = Overflow Must be manually cleared by triggering another conversion or by clearing the accumulators with the RSTACC bit. |
8 | RESERVED | R | 0h | Reserved. Always read 0. |
7 | TMPOL | R/W | 0h | This bit is set to 1 if the temperature measurement
exceeds the threshold limit in the temperature over-limit register.
0h = Normal 1h = Overtemperature Event When ALATCH =1 this bit is cleared by reading this register. |
6 | CURRENTOL | R/W | 0h | This bit is set to 1 if the current measurement
exceeds the threshold limit in the current over-limit register. 0h = Normal 1h = Overcurrent Event When ALATCH =1 this bit is cleared by reading this register. |
5 | CURRENTUL | R/W | 0h | This bit is set to 1 if the current measurement falls
below the threshold limit in the current under-limit register. 0h = Normal 1h = Undercurrent Event When ALATCH =1 this bit is cleared by reading this register. |
4 | BUSOL | R/W | 0h | This bit is set to 1 if the bus voltage measurement
exceeds the threshold limit in the bus over-limit register. 0h = Normal 1h = Bus Over-Limit Event When ALATCH =1 this bit is cleared by reading this register. |
3 | BUSUL | R/W | 0h | This bit is set to 1 if the bus voltage measurement
falls below the threshold limit in the bus under-limit register. 0h = Normal 1h = Bus Under-Limit Event When ALATCH =1 this bit is cleared by reading this register. |
2 | POL | R/W | 0h | This bit is set to 1 if the power measurement exceeds
the threshold limit in the power limit register. 0h = Normal 1h = Power Over-Limit Event When ALATCH =1 this bit is cleared by reading this register. |
1 | CNVRF | R/W | 0h | This bit is set to 1 if the conversion is completed.
0h = Normal 1h = Conversion is complete When ALATCH =1 this bit is cleared by reading this register or starting a new triggered conversion. |
0 | MEMSTAT | R/W | 1h | This bit is set to 0 if a checksum error is detected
in the device trim memory space. 0h = Memory Checksum Error 1h = Normal Operation |
If negative values are entered in this register, then a current measurement of 0 A will trip this alarm. When using negative values for the undercurrent and overcurrent thresholds be aware that the overcurrent threshold must be set to the larger (that is, less negative) of the two values. The COL register is shown in Table 7-16.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | COL | R/W | 7FFFh | Sets the threshold for comparison of the value to detect over current condition (overcurrent protection). Two's complement value. Conversion factor: 1.2 mA/LSB |
The CUL register is shown in Table 7-17.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | CUL | R/W | 8000h | Sets the threshold for comparison of the value to detect undercurrent condition. Two's complement value. Conversion factor: 1.2 mA/LSB |
The BOVL register is shown in Table 7-18.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | Reserved | R | 0h | Reserved. Always reads 0. |
14-0 | BOVL | R/W | 7FFFh | Sets the threshold for comparison of the value to
detect Bus Overvoltage (overvoltage protection). Unsigned
representation, positive value only. Conversion factor: 3.125
mV/LSB. |
The BUVL register is shown in Table 7-19.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15 | Reserved | R | 0h | Reserved. Always reads 0. |
14-0 | BUVL | R/W | 0h | Sets the threshold for comparison of the value to
detect Bus Undervoltage (undervoltage protection). Unsigned
representation, positive value only. Conversion factor: 3.125
mV/LSB. |
The TEMP_LIMIT register is shown in Table 7-20.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-4 | TOL | R/W | 7FFh | Sets the threshold for comparison of the value to
detect over temperature measurements. Two's complement value. The value entered in this field compares directly against the value from the DIETEMP register to determine if an overtemperature condition exists. Conversion factor: 125 m°C/LSB. |
3-0 | Reserved | R | 0 | Reserved, always reads 0 |
The PWR_LIMIT register is shown in Table 7-21.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | POL | R/W | FFFFh | Sets the threshold for comparison of the value to
detect power over-limit measurements. Unsigned representation,
positive value only. The value entered in this field compares directly against the value from the POWER register to determine if an over-power condition exists. Conversion factor: 256 × Power LSB or 61.44 mW/LSB |
The MANUFACTURER_ID register is shown in Table 7-22.
Return to the Summary Table.
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
15-0 | MANFID | R | 5449h | Reads back TI in ASCII. |