JAJSD55A May 2017 – June 2017 INA826S
PRODUCTION DATA.
The INA826S operates over a power-supply range of 3 V to 36 V (±3 V to ±18 V). Supply voltages higher than 40 V (±20 V) can permanently damage the device. Parameters that vary over supply voltage or temperature are illustrated in the Typical Characteristics section.
The INA826S can operate on power supplies as low as 3 V. Most parameters vary only slightly throughout this supply voltage range; see the Typical Characteristics section. Operation at very low supply voltage requires careful attention to assure that the input voltages remain within the linear range. Voltage swing requirements of internal nodes limit the input common-mode range with low power-supply voltage. The typical characteristic curves Figure 12 through Figure 18 and Figure 44 through Figure 46 describe the range of linear operation for various supply voltages, reference connections, and gains.