SBOS631B June 2012 – November 2017 INA827
PRODUCTION DATA.
The INA827 is a monolithic instrumentation amplifier (INA) based on a 36-V and a current feedback input architecture. The INA827 also integrates laser-trimmed resistors to ensure excellent common mode rejection and low gain error. The combination of the current feedback input and the precision resistors allows this device to achieve outstanding dc precision as well as frequency response and high frequency common mode rejection(TBD this is more like a Layout text. Overview is generally an overview of the device.)
The Overview section provides a top-level description of what the device is and what it does. Detailed descriptions of the features and functions appear in subsequent subsections. Guidelines ● Include a summary of standards met by the device (if any). ● List modes and states of operation (from the user's perspective) and key features within each functional mode for quick reference. Use the following sections to provide detail on these modes and features.
Device gain is set by a single external resistor (RG), connected between pins 2 and 3. The value of RG is selected according to Equation 1:
Table 1 lists several commonly-used gains and resistor values. The on-chip resistors are laser-trimmed to accurate absolute values. The accuracy and temperature coefficients of these resistors are included in the gain accuracy and drift specifications of the INA827.
DESIRED GAIN (V/V) | RG (Ω) | NEAREST 1% RG (Ω) |
---|---|---|
5 | — | — |
10 | 16.00k | 15.8k |
20 | 5.333k | 5.36k |
50 | 1.778k | 1.78k |
100 | 842.1 | 845 |
200 | 410.3 | 412 |
500 | 161.6 | 162 |
1000 | 80.40 | 80.6 |
The stability and temperature drift of the external gain setting resistor (RG) also affects gain. The RG contribution to gain accuracy and drift can be directly inferred from the gain of Equation 1.
The best gain drift of 1 ppm per degree Celsius can be achieved when the INA827 uses G = 5 without RG connected. In this case, the gain drift is limited only by the slight temperature coefficient mismatch of the integrated 50-kΩ resistors in the differential amplifier (A3). At gains greater than 5, the gain drift increases as a result of the individual drift of the resistors in the feedback of A1 and A2, relative to the drift of the external gain resistor RG. Process improvements to the temperature coefficient of the feedback resistors now enable a maximum gain drift of the feedback resistors to be specified at 35 ppm per degree Celsius, thus significantly improving the overall temperature stability of applications using gains greater than 5.
Low resistor values required for high gains can make wiring resistance important. Sockets add to wiring resistance and contribute additional gain error (such as possible unstable gain errors) at gains of approximately 100 or greater. To ensure stability, avoid parasitic capacitances greater than a few picofarads at RG connections. Careful matching of any parasitics on both RG pins maintains optimal CMRR over frequency; see the Typical Characteristics section.
Most applications require no external offset adjustment; however, if necessary, adjustments can be made by applying a voltage to the REF pin. Figure 56 shows an optional circuit for trimming the output offset voltage. The voltage applied to the REF pin is summed at the output. The op amp buffer provides low impedance at the REF pin to preserve good common-mode rejection.
The linear input voltage range of the INA827 input circuitry extends from the negative supply voltage to 1 V below the positive supply, and maintains 88-dB (minimum) common-mode rejection throughout this range. The common-mode range for most common operating conditions is described in Figure 14 and Figure 35 through Figure 38. The INA827 can operate over a wide range of power supplies and VREF configurations, thus making a comprehensive guide to common-mode range limits for all possible conditions impractical to provide.
The most commonly overlooked overload condition occurs when a circuit exceeds the output swing of A1 and A2, which are internal circuit nodes that cannot be measured. Calculating the expected voltages at the output of A1 and A2 (see Figure 57) provides a check for the most common overload conditions. The A1 and A2 designs are identical and the outputs can swing to within approximately 100 mV of the power-supply rails. For example, when the A2 output is saturated, A1 can continue to be in linear operation and responding to changes in the noninverting input voltage. This difference can give the appearance of linear operation but the output voltage is invalid.
A single-supply instrumentation amplifier has special design considerations. To achieve a common-mode range that extends to single-supply ground, the INA827 employs a current-feedback topology with PNP input transistors; see Figure 57. The matched PNP transistors (Q1 and Q2) shift the input voltages of both inputs up by a diode drop and (through the feedback network) shift the output of A1 and A2 by approximately +0.8 V. With both inputs and VREF at single-supply ground (negative power supply), the output of A1 and A2 is well within the linear range, allowing differential measurements to be made at the GND level. As a result of this input level-shifting, the voltages at pins 2 and 3 are not equal to the respective input pin voltages (pins 1 and 4). For most applications, this inequality is not important because only the gain-setting resistor connects to these pins.
See Figure 61 for a simplified representation of the INA827. A more detailed diagram (shown in Figure 57) provides additional insight into the INA827 operation.
Each input is protected by two field-effect transistors (FETs) that provide a low series resistance under normal signal conditions and preserve excellent noise performance. When excessive voltage is applied, these transistors limit input current to approximately 8 mA.
The differential input voltage is buffered by Q1 and Q2 and is applied across RG, causing a signal current to flow through RG, R1, and R2. The output difference amplifier (A3) removes the common-mode component of the input signal and refers the output signal to the REF pin.
The equations shown in Figure 57 describe the output voltages of A1 and A2. The VBE and voltage drop across R1 and R2 produce output voltages on A1 and A2 that are approximately 0.8 V higher than the input voltages.
The INA827 inputs are individually protected for voltages up to ±40 V. For example, a condition of –40 V on one input and +40 V on the other input does not cause damage. However, if the input voltage exceeds [(V–) – 2 V] and the signal source current drive capability exceeds 3.5 mA, the output voltage switches to the opposite polarity; see Figure 14. This polarity reversal can easily be avoided by adding a 10-kΩ resistance in series with both inputs.
Internal circuitry on each input provides low series impedance under normal signal conditions. If the input is overloaded, the protection circuitry limits the input current to a safe value of approximately 8 mA. Figure 14 illustrates this input current limit behavior. The inputs are protected even if the power supplies are disconnected or turned off.
The INA827 input impedance is extremely high—approximately 20 GΩ. However, a path must be provided for the input bias current of both inputs. This input bias current is typically 35 nA. High input impedance means that this input bias current changes very little with varying input voltage.
Input circuitry must provide a path for this input bias current for proper operation. Figure 58 shows various provisions for an input bias current path. Without a bias current path, the inputs float to a potential that exceeds the INA827 common-mode range, and the input amplifiers saturate. If the differential source resistance is low, the bias current return path can be connected to one input (as shown in the thermocouple example in Figure 58). With higher source impedance, using two equal resistors provides a balanced input with possible advantages of lower input offset voltage as a result of bias current and better high-frequency common-mode rejection.
The INA827 output voltage is developed with respect to the voltage on the reference pin. Often, in dual-supply operation, the reference pin (pin 6) is connected to the low-impedance system ground. Offsetting the output signal to a precise mid-supply level (for example, 2.5 V in a 5-V supply environment) can be useful in single-supply operation. The signal can be shifted by applying a voltage to the device REF pin, which can be useful when driving a single-supply ADC.
For best performance, keep any source impedance to the REF pin below 5 Ω. Referring to Figure 61, the reference resistor is at one end of a 50-kΩ resistor. Additional impedance at the REF pin adds to this 50-kΩ resistor. The imbalance in resistor ratios results in degraded common-mode rejection ratio (CMRR).
Figure 59 shows two different methods of driving the reference pin with low impedance. The OPA330 is a low-power, chopper-stabilized amplifier and therefore offers excellent stability over temperature. The OPA330 is available in the space-saving SC70 and even smaller chip-scale package. The REF3225 is a precision reference in a small SOT23-6 package.
Figure 19 illustrates that, despite having low quiescent current of only 200 µA, the INA827 achieves much wider bandwidth than other instrumentation amplifiers (INAs) in its class. This achievement is a result of using TI’s proprietary high-speed precision bipolar process technology. The current-feedback topology provides the INA827 with wide bandwidth even at high gains. Settling time also remains excellent at high gain because of a 1.5-V/µs high slew rate.
The INA827 operates over a power-supply range of +3 V to +36 V (±1.5 V to ±18 V). Supply voltages higher than 40 V (±20 V) can permanently damage the device. Parameters that vary over supply voltage or temperature are shown in the Typical Characteristics section.
The INA827 can operate on power supplies as low as ±1.5 V. Most parameters vary only slightly throughout this supply voltage range; see the Typical Characteristics section. Operation at very low supply voltage requires careful attention to assure that the input voltages remain within the linear range. Voltage swing requirements of the internal nodes limit the input common-mode range with low power-supply voltage. Figure 7 to Figure 13 and Figure 35 to Figure 38 describe the linear operation range for various supply voltages, reference connections, and gains.
Most modern signal-conditioning systems calibrate errors at room temperature. However, calibration of errors that result from a change in temperature is normally difficult and costly. Therefore, these errors must be minimized by choosing high-precision components such as the INA827 that have improved specifications in critical areas that effect overall system precision. Figure 60 shows an example application.
Resistor-adjustable INAs such as the INA827 yield the lowest gain error at G = 5 because of the inherently well-matched drift of the internal resistors of the differential amplifier. At gains greater than 5 (for instance, G = 10 V/V or G = 100 V/V) gain error becomes a significant error source because of the resistor drift contribution of the feedback resistors in conjunction with the external gain resistor. Except for very high gain applications, gain drift is by far the largest error contributor compared to other drift errors (such as offset drift). The INA827 offers the lowest gain error over temperature in the marketplace for both G > 5 and G = 5 (no external gain resistor). Table 2 summarizes the major error sources in common INA applications and compares the two cases of G = 5 (no external resistor) and G = 10 (with a 16-kΩ external resistor). As shown in Table 2, although the static errors (absolute accuracy errors) in G = 5 are almost twice as great as compared to G = 10, there is a great reduction in drift errors because of the significantly lower gain error drift. In most applications, these static errors can readily be removed during calibration in production. All calculations refer the error to the input for easy comparison and system evaluation.
ERROR SOURCE | ERROR CALCULATION | INA827 | ||
---|---|---|---|---|
SPECIFICATION | G = 10 ERROR (ppm) | G = 1 ERROR (ppm) | ||
ABSOLUTE ACCURACY AT +25°C | ||||
Input offset voltage (µV) | VOSI / VDIFF | 150 | 150 | 150 |
Output offset voltage (µV) | VOSO / (G × VDIFF) | 2000 | 200 | 400 |
Input offset current (nA) | IOS × maximum (RS+, RS–) / VDIFF | 5 | 50 | 50 |
CMRR (dB) | VCM / (10CMRR / 20 × VDIFF) | 94 (G = 10), 88 (G = 5) |
200 | 398 |
Total absolute accuracy error (ppm) | 600 | 998 | ||
DRIFT TO +105°C | ||||
Gain drift (ppm/°C) | GTC × (TA – 25) | 25 (G = 10), 1 (G = 5) |
2000 | 80 |
Input offset voltage drift (μV/°C) | (VOSI_TC / VDIFF) × (TA – 25) | 5 | 200 | 200 |
Output offset voltage drift (μV/°C) | [VOSO_TC / ( G × VDIFF)] × (TA – 25) | 30 | 240 | 240 |
Total drift error (ppm) | 2440 | 760 | ||
RESOLUTION | ||||
Gain nonlinearity (ppm of FS) | 5 | 5 | 5 | |
Voltage noise (1 kHz) | ![]() |
eNI = 17 eNO = 250 |
6 | 6 |
Total resolution error (ppm) | 11 | 11 | ||
TOTAL ERROR | ||||
Total error | Total error = sum of all error sources | 3051 | 1769 |
The INA827 has a single functional mode and is operational when the power-supply voltage is greater than 3 V (±1.5 V). The maximum power-supply voltage for the INA827 is 36 V (±18 V).