SLLSER5 December 2015 ISO7142CC-Q1
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The ISO7142CC-Q1 device uses single-ended TTL-logic switching technology. The supply voltage range is from 2.7 V to 5.5 V for both supplies, VCC1 and VCC2. When designing with digital isolators, keep in mind that because of the single-ended design structure the single-ended design structure, digital isolators do not conform to any specific interface standard and are only intended for isolating single-ended CMOS or TTL digital signal lines. The isolator is typically placed between the data controller (that is, µC or UART), and a data converter or a line transceiver, regardless of the interface type or standard.
Figure 15 shows the typical isolated CAN interface implementation.
Unlike optocouplers, which require external components to improve performance, provide bias, or limit current, the ISO7142CC-Q1 device only requires two external bypass capacitors to operate.
Figure 16 shows the hookup of a typical ISO7142CC-Q1 circuit. The only external components are two bypass capacitors.