JAJSPG2A December 2022 – March 2024 IWRL6432
PRODUCTION DATA
The following the system topologies are supported.
In Topology 1: Autonomous mode, the IWRL6432 can be used as full sensor along with M4F application processor. In this case the internal application processor does all the processing and interrupts the host processor to communicate to take action based on the sensor data. Most of the processing happens on the internal MCU of the IWRL6432 chip and only high level desired results are communicated to external host. In this topology MIPS, processing capability on the external MCU is relaxed and very low cost and low power MCU can be used.
In Topology 2: Peripheral mode, the IWRL6432 is controlled by external MCU and most of the processing is done on external MCU. In this case computational and power requirements are higher and the external MCU stays active most of the time.