JAJSI72 November 2019 LDC1001
PRODUCTION DATA.
An AC current flowing through an inductor will generate an AC magnetic field. If a conductive material, such as a metal target, is brought into the vicinity of the coil, this magnetic field will induce circulating currents (eddy currents) on the surface of the target. These eddy currents are a function of the distance, size, and composition of the target. The eddy currents then generate their own magnetic field, which opposes the original field generated by the coil. This mechanism is best compared to a transformer, where the coil is the primary core and the eddy current is the secondary core. The inductive coupling between both cores depends on distance and shape. Hence the resistance and inductance of the secondary core (eddy current), shows up as a distant dependent resistive and inductive component on the primary side (coil). Figure 5 and Figure 8 show a simplified circuit model.
Figure 5. Inductor With a Metal Target Eddy currents generated on the surface of the target can be modeled as a transformer as shown in Figure 6. The coupling between the primary and secondary coils is a function of the distance and the characteristics of the conductor. In Figure 6, the inductance LS is the inductance of the coil, and RS is the parasitic series resistance of the coil. The inductance L(d), which is a function of sensor to target distance, d, is the coupled inductance of the metal target. Likewise, R(d) is the parasitic resistance of the eddy currents and is also a function of distance.
Figure 6. Metal Target Modeled as L and R With Circulating Eddy Currents Generating an alternating magnetic field with just an inductor will consume a large amount of power. This power consumption can be reduced by adding a parallel capacitor, turning it into a resonator as shown in Figure 7. In this manner the power consumption is reduced to the eddy and inductor losses RS + R(d) only.
Figure 7. LC Tank Connected to Oscillator The LDC1001 doesn’t measure the series resistance directly; instead it measures the equivalent parallel resonance impedance RP (see Figure 8). This representation is equivalent to the one shown in Figure 8, where the parallel resonance impedance RP(d) is given by Equation 1:
Figure 8. Equivalent Resistance of RS in Parallel With LC Tank Figure 9 shows the variation in RP as a function of distance for a 14-mm diameter PCB coil (refer to the sensor characteristics in Table 23). The target in this example is a section of a 2-mm thick stainless steel disk.
Figure 9. Typical RP vs Distance With 14-mm PCB Coil