JAJSI72 November 2019 LDC1001
PRODUCTION DATA.
The LDC1001 supports a wide range of LC combinations, with oscillation frequencies ranging from 5 kHz to 5 MHz and RP ranging from 798 Ω to 3.93 MΩ. This range of RP can be viewed as the maximum input range of an ADC. As shown in Figure 9, the range of RP is typically much smaller than the maximum input range supported by the LDC1001. To get better resolution in the desired sensing range, the LDC1001 offers a programmable input range through the RP_MIN and RP_MAX registers. Refer to Calculation of RP_MIN and RP_MAX for information on setting these registers.
When the resonance impedance RP of the sensor drops below the programed RP_MIN, the RP output of the LDC will clip at its full scale output. This situation could, for example, happen when a target comes too close to the coil.
Use Equation 2 to calculate the resonance impedance from the digital output code:
where
Example: If Proximity data (address 0x22:0x21) is 5000, RP_MIN is 2.394 kΩ, and RP_MAX is 38.785 kΩ ,the resonance impedance is given by:
Y = 5000/215 = 0.1526
RP = (38785 × 2394) ÷ (2394 × (1 – 0.1526) + 38785 × 0.1526) = (92851290 ÷ (2028.675 + 5918.591))
RP = 11.683 kΩ