JAJSGO3C december 2018 – july 2023 LDC5072-Q1
PRODUCTION DATA
To set the gain of the final gain stage, a voltage in the range of VAGC_EN_MANUAL must be applied to the AGC_EN pin. This gain setting will be set during the DIAGNOSTICS state. A change in the voltage on AGC_EN affects the AGC gain the next time the device enters the DIAGNOSTICS state, either during the next power up of the device or during fault recovery. The nominal value of minimum gain of this stage is 0.375 and the maximum gain is 60.375. The gain is implemented as linear in dB scale with 256 steps. This gain is rotation frequency dependent. For higher rotation speeds, the gain value will fall off. Equation 7 shows the gain in linear scale is related to the voltage on AGC_EN pin as a percentage of VREG:

where
The voltage applied on AGC_EN pin should fall within VAGC_EN_MANUAL range.